Technical FAQs

Ask a Question

Does Square D offer a 400 amp, Ring type three phase or single phase, EZM Branch Device?

Issue:
Product availability

Product Line:
EZM Metering

Environment:
Meter Socket design 

Cause:
Customer request

Resolution:

Square D does NOT offer a Ring Type, 400amp, EZM Branch device. This is not a common device the industry uses or utility companies require.


CTA-ID : 2020923
Was this helpful?
What can we do to improve the information ?