Technical FAQs

Ask a Question

Where are 2nd. set of tightening screws on LBA365212 pictured on Digest 173 page 22-18?

They are down in the recessed area and are out of view in the picture.

This is not a FAQ question


CTA-ID : 2020921
Was this helpful?
What can we do to improve the information ?