Technical FAQs

Ask a Question

The warranty sheet that came with the SDSB1175C says to use it in conjunction with a UL 1449 device. What does this mean?

The warranty document states that when the SDSB1175C is used with a point of use UL1449 (plug strip type device) or used with a QO or HOM load center then the warranty amount is increased up to $50,000.00 or the users home owner insurance deductable. It is not required to use a point of use plug strip for the basic $25,000.00 warranty to be valid.

CTA-ID : 2020419
Was this helpful?
What can we do to improve the information ?