Technical FAQs

Ask a Question

What terminals are used for the 4-20ma external signal to the 8839 58M enclosed drive?

The positive side goes to G1, S2+ which is AI2 on the drive (Analog Input 2: Speed Reference Voltage). The negative side goes to J, S3 which is COM (Speed Reference Common).

CTA-ID : 2020416
Was this helpful?
What can we do to improve the information ?