Technical FAQs

Ask a Question

What is the manual transfer kit for QO816L100F, QO816L100S or QO816L100RB load center?

Issue:
Selection

Product Line:
QO LC Accessory

Cause:
Selection

Resolution:
If the application is to assure that two breakers are interlocked to allow only one of them to feed their load at one time, use QO2DTI. 
If the application is back feeding two breakers from two separate sources, use QO2DTIM. The QO2DTIM includes the QO2DTI interlock and (2) PK2MB breaker retainers.


CTA-ID : 2020413
Was this helpful?
What can we do to improve the information ?