Technical FAQs

Ask a Question

What is the magnetic trip setting for MAL36900?

The AC magnetic trip setting is:
Low = 4500
High = 9000
(UL magnetic trip setting tolerances are + or - 25%(low) and + or - 20%(High) from nominal values shown)


CTA-ID : 2020680
Was this helpful?
What can we do to improve the information ?