Technical FAQs

Ask a Question

What are the replacement parts for an H227AWK Series E4 Heavy Duty Safety Switch?

The parts listed here are the only field replaceable parts on the H227AWK, series E4:
LINE BASE - ORDER THE FOLLOWING:
---Line Base Assembly - 4401119750 (qty 1 per phase, includes Lug)
---Line Base Insulating Plug - 4401133901 (qty 3 per phase)
---Base Mounting Screw - 4020600901 (qty 3 per phase)
---Line Base Phase Barrier - 4401119501 (qty 2 total)
LOAD BASE - ORDER THE FOLLOWING:
---Load Base Assembly - 4401120050 (qty 1 per phase, Lug not included)
---Lug -4405005302 (qty 1 per phase)
---Lug Mounting Nut - 2342702400 (qty 1 per phase)
---Base Mounting Screw - 4020600901 (qty 2 per phase)
LINE AND LOAD LUG - ORDER THE FOLLOWING:
---Lug - 4405005302 (qty 1 per wire)
---Lug Mounting Nut - 2342702400 (qty 1 per wire)
CROSSBAR INSULATOR - ORDER THE FOLLOWING:
---Crossbar Insulator Kit - 4051275250 (note: the metal cross bar is not replaceable)
HANDLE ASSEMBLY - ORDER THE FOLLOWING:
---Handle Assembly - 4401141350 (qty 1, includes Handle Knob)
---Handle Assembly Mounting Bolt - 2140122242 (qty 2)
---Handle Assembly Lock Washer - 2370200221 (qty 2)
HANDLE KNOB - ORDER THE FOLLOWING:
---Red Knob - 4052085701 (qty 1)
---Black Knob - 4052085702 (qty 1)
---Rivet - 2410108441 (qty 2)
DOOR THUMB SCREWS - ORDER THE FOLLOWING:
---Door Thumb Screw - 4405043401 (qty 3)
---Door Thumb Screw Retainer - 4405049001 (qty 3)


CTA-ID : 2020406
Was this helpful?
What can we do to improve the information ?