Technical FAQs

Ask a Question

Are the Class 9421 Type D10* disconnect switches finger safe?<br />* S1, S2, S3, S4, S1H, S2H, S3H, S4H

No, however they provide Dead-Front construction which means when the switch is in the off position, all visable current carrying parts are de-energized , thus providing additional safety.


CTA-ID : 2020401
Was this helpful?
What can we do to improve the information ?