Technical FAQs

Ask a Question

Why does the SSL parameter not appear in the ATV31 drC menu and parameter SrF appears instead?

SSL has been renamed to SrF.  SRF is a speed loop filter which can be suppressed only to reduce the speed response time slightly for critical applications which need good positionning performances.

Reviewed 6/2011

CTA-ID : 2020339
Was this helpful?
What can we do to improve the information ?