Technical FAQs

Ask a Question

What is the undervoltage threshold for the 460vac ATV58 drives?

It is 360Vdc or 267Vac(360/1.35). The drive will reset the fault at 460Vdc or 341Vac.


CTA-ID : 2020295
Was this helpful?
What can we do to improve the information ?