Technical FAQs

Ask a Question

Does the ANSI Masterpact NW breaker have a grounded B phase rating?

The ANSI standard does not address grounded B phase ratings. However, ANSI C37 does require single phase tests at 87% of the full AIR of the breaker, which is the theoretical maximum single phase current that could flow.

CTA-ID : 2020639
Was this helpful?
What can we do to improve the information ?