Technical FAQs

Ask a Question

What is the replacement spring charging motor for SED and SEF breakers?<br />

Advised we have 4 depending on the control voltage
120VAC = S3MOT120AC2
24VDC = S3MOT024DC2
48VDC = S3MOT048DC2
125VDC = S3MOT125DC2

Note that these motors cannot be added to a breaker that did not come from the factory with one.



CTA-ID : 2020636
Was this helpful?
What can we do to improve the information ?