Technical FAQs

Ask a Question

Is there an enclosure available for the MAL261200, MHL261200, MAL361200 or MHL361200 ?

There are no individual enclosures for the 1200 ampere MAL/MHL circuit breaker for use on AC voltages. The MA1200S is available for 1200A maximum, 500VDC maximum applications only.

CTA-ID : 2020362
Was this helpful?
What can we do to improve the information ?