Technical FAQs

Ask a Question

Is there a difference between constant torque and variable torque ratings with the Altivar 31?

No. The ATV31 drives are rated for Variable Torque and for Constant Torque.
There is no need to derate the drive for either torque type.

CTA-ID : 2020879
Was this helpful?
What can we do to improve the information ?