Technical FAQs

Ask a Question

Is the GJL Mag-Gard circuit breaker UL listed, CSA Certified?

The GJL Mag-Gard circuit breaker is a UL489 Recognized Component. Recognized uner UL file E113389 and Certified under CSA file LR 69561.


CTA-ID : 2020606
Was this helpful?
What can we do to improve the information ?