Technical FAQs

Ask a Question

What type of material is used for the boot on the 9007MS10.../9007MS12.../9007MS13... booted limit switch?

It is Buna-N.


CTA-ID : 2021281
Was this helpful?
What can we do to improve the information ?