Technical FAQs

Ask a Question

Are both endwalls blank for an MH674 box?

Issue:
Are the end walls on a MH674 blank?

Product Line:
NQOD Enclosure and Accessories

Environment:
Products sold in North America

Cause:
Need to know conduit options for a NQOD 600A main breaker panel.

Resolution:
Yes, the end walls on the MH674 are blank. This MH674 and blank end wall (80110-319-01) replacement are obsolete.

CTA-ID : 2021272
Was this helpful?
What can we do to improve the information ?