Technical FAQs

Ask a Question

Customer asks what type of enclosure does the 3kVA buck boost transformer have? (3S43F, 3S46F, 3S82F)

The enclosure is not unlike the 10A enclosure (encapsulated, wall mounting, NEMA 3R) on page 12-10 of Digest 173, only with different dimensions of 14.5``H x 8.6``W x 6.5``D.

CTA-ID : 2021269
Was this helpful?
What can we do to improve the information ?