Technical FAQs

Ask a Question

Does the enclosure MH674 have Knockouts or blank endwalls?

Issue:
Does the enclosure MH674 have Knockouts or blank endwalls?

Product Line:
NQOD Enclosure and Accessories

Environment:
Products sold in North America

Cause:
Need to know conduit options for a NQOD 600A main breaker panel.

Resolution:
The MH674 has endwalls are blank with no knockouts.

The MH674 and blank end wall (80110-319-01) replacement are obsolete.


CTA-ID : 2021088
Was this helpful?
What can we do to improve the information ?