Technical FAQs

Ask a Question

What is the horsepower rating of HU364DS safety switch?

It is rated at 15 HP at 240v single phase, 60HP at 240v three phase, 50 HP at 480v single phase, 125 HP at 480v three phase, 50 HP at 600v single phase and 150 HP at 600v three phase. The HP ratings applicable for a safety switch are printed on the Wiring Diagram, located inside the front cover of the switch.



CTA-ID : 2021086
Was this helpful?
What can we do to improve the information ?