Technical FAQs

Ask a Question

What are the dimensions and weight for the ATV58HU29M2, ATV58HU41M2, ATV58HU18N4, ATV58HU29N4, ATV58HU41N4?

Width is 5.91 inches (150mm)
Depth is 7.24 inches (184mm)
Height is 9.06 inches (230mm)
The weight is 8.4lbs (3.8kg)


CTA-ID : 2020865
Was this helpful?
What can we do to improve the information ?