Technical FAQs

Ask a Question

Is the GJL thermal-magnetic circuit breaker UL listed?

Yes, the thermal-magnetic GJL circuit breaker is built and tested in accordance with UL489 Standards and CSA Standards C22.2 No. 5.1 Standard. UL file E63335 and CSA file LR 69561.

CTA-ID : 2020604
Was this helpful?
What can we do to improve the information ?