Technical FAQs

Ask a Question

What is the differential of an XMLF pressure switch?

The differential varies within the range of the device and is depicted in a graph associated with the XMLF catalog depiction.  
The minimum differential of an XMLF electronic pressure switch is 3% of the range.  
Example: Range is 0-145 psi the min differential would be 4.35 psi.


CTA-ID : 2021253
Was this helpful?
What can we do to improve the information ?