Technical FAQs

Ask a Question

What are the replacement incandescent lamps for an XVAC or XVAL indicating bank or beacon?<br /><br />

Voltage AC/DC Wattage Lamp Part Number
12 2.5 DL1BA012
24 4.0 DL1BA024
24 6.5 DL1BL024
48 4.0 DL1BA048
110 7.0 DL1BA110
120 7.0 DL1BL120
160 5.0 DL1BA160
240 6.0 DL1BA260
These are a BA15d bayonet style lamp. The BL versions are 49 mm tall and the BA versions are 41 mm tall.


CTA-ID : 2020851
Was this helpful?
What can we do to improve the information ?