Technical FAQs

Ask a Question

Can the 92355R be used on a 208v system? (Footnote says 240v only)

Yes, 208v is an acceptable voltage. The footnote is referring to the maximum voltage of 240VAC and the fact that 250VDC is not allowed.



CTA-ID : 2020584
Was this helpful?
What can we do to improve the information ?