Technical FAQs

Ask a Question

What is a PGC, PJC, PLC circuit breaker?

It is ``slang`` for a PG, PF, or PL breaker that is 100% rated. The ``C`` actually resides farther down in the catalog number just before the trip unit designation. The ``C`` denotes a 100% rating, not a connection type.

CTA-ID : 2012363
Was this helpful?
What can we do to improve the information ?