Technical FAQs

Ask a Question

What does the P mean on an FAP34100 breaker?

The P in the third position means no lugs on the ``ON`` end and lugs on the ``OFF`` end. If there is a P in the third position and an MT at the end of the part number the situation is reversed and there are lugs on the ``ON`` end but no lugs on the ``OFF`` end.


CTA-ID : 15981
Was this helpful?
What can we do to improve the information ?