Technical FAQs

Ask a Question

What is the NEMA rating for a PQ4606G?

The Plug-in units are rated for indoor use only. This rating is similar to NEMA 1.


CTA-ID : 2021047
Was this helpful?
What can we do to improve the information ?