Technical FAQs

Ask a Question

Can the ATV58 115VAC I-O Option kit part number VW3A58275U be installed on a drive that also has a serial communications card installed?

Yes. The I-O converter does not interfere with the mounting of the other option card. The VW3A58275U connects to the 10 pin I-O terminals that are on the bottom of the main control board. Serial communication cards mount to the front of the main control board.


CTA-ID : 2020648
Was this helpful?
What can we do to improve the information ?