Technical FAQs

Ask a Question

Are the 9007MS limit switches available without cable?<br />

Yes, there are several plug type options. See Digest 173 page 19-26 for general options selection.



CTA-ID : 2021037
Was this helpful?
What can we do to improve the information ?