Technical FAQs

Ask a Question

Customer wants an R frame Powerpact breaker with ground fault alarm without tripping.

Use 5.0P trip unit (LSI functions). Set alarm up via trip unit protection menu. Use 2PCM programmable contact module for output. Need neutral CT if it is a 4 wire system.
Use 5.0P trip unit (LSI functions). Set alarm up via trip unit Amperage Protection menu (trip curve button). Then set up S1 or S2 contact on 2PCM programmable contact module in MAINTENANCE menu (wrench button). Need neutral CT if it is a 4 wire system.


CTA-ID : 2019287
Was this helpful?
What can we do to improve the information ?