Technical FAQs

Ask a Question

What is the ambient temperature rating for the 2510 Type F manual starters and Type K switches?

The ambient temperature rating is 0-40 degrees C.


CTA-ID : 2019283
Was this helpful?
What can we do to improve the information ?