Technical FAQs

Ask a Question

What are the repair parts for a RC816D150C Series 002?

Issue:
Repair parts

Product Line:
CSED

Environment:
Repair parts

Cause:
Maintenance

Resolution:
The parts listed here are the only field replaceable parts.
Rainproof Cap - 40561-158-03 (This is the top cap that covers the top endwall of the device)
Rainproof Cap Mounting Screws - (2) 21427-17161
Meter Cover - 40561-430-52
Load Center Cover - 40561-280-52
Dead Front Cover - 40561-145-02
Load Center Interior (8-16 ckt branch breaker base) - 40561-333-52 (Does not include main breaker, order separately)
Main Breaker - HOM2150
Main Breaker Hold-Down Strap - 40561-327-01
Secondary Main Breaker Mounting Base (for 2-Pole HOM) - 40558-417-51
Meter Base assembly - 40561-494-52
Meter Jaw - 40527-069-50 (OBSOLETE - REPLACED BY 73297-948-50)
Meter Jaw Blade Guide - 40527-619-01


CTA-ID : 2019280
Was this helpful?
What can we do to improve the information ?