Technical FAQs

Ask a Question

On a UFP222RGFI, is a separate circuit required to feed the GFCI receptacle?

Yes, two circuits are required when using the UFP222RGFI. First, a 240Vac, 60A max, power circuit is required to feed the load equipment (air conditioner, air handling unit, water heater, etc.). Secondly, a 125V, 20A, circuit is required to feed the GFCI receptacle.


CTA-ID : 2020277
Was this helpful?
What can we do to improve the information ?