Technical FAQs

Ask a Question

On a UFP222RD, does removing the pullout disconnect both the power circuit and the receptacle circuit?

The UFP222RD pullout disconnects the 240Vac power circuit only. It does not control the 120Vac receptacle circuit. The receptacle should be controlled by the circuit breaker feeding the receptacle circuit.


CTA-ID : 2020274
Was this helpful?
What can we do to improve the information ?