Technical FAQs

Ask a Question

Can the knob on the XB4BT42 be replaced?

Issue:
The replacement of a 22mm mushroom knob is being requested to be ordered.

Product Line:
22mm push button

Environment:
Non-illuminated Emergency Stop and Emergency Off Mushroom Head Push Button

Cause:
Existing emergency push button head needs to be replaced.

Resolution:
The knobs on the XB4 and XB5 operators are not replaceable. Must order new complete operator.
 
Was this helpful?
What can we do to improve the information ?