Technical FAQs

Ask a Question

Are alternate mechanical lugs available for the EZM3600CB?

Issue:
Product Design Features


Product Line:
EZM Metering Equipment

Environment:
Alternate Main Lugs

Cause:
Application

Resolution:

Yes, the standard mechanic lugs will accommodate (3) 500 Kcmil Al/Cu wires maximum per phase and neutral.
1) For (2) 600 Kcmil Al/Cu wires Maximum per phase and neutral use the lug kit AL800MA7 for the Main breaker and the lug kit MMLK250 for the main neutral.
2) For (2) 750 Kcmil Al/Cu wires Maximum per phase and neutral use the lug kit AL800MA7 for the Main breaker and the lug kit MMSK2 and the TA8002N ILSO Lugs (Purchased separate) for the main neutral.
3) For (4) 350 Kcmil Al/Cu wires Maximum per phase and neutral use the lug kit AL1000MA for the main breaker and the standard neutral Lugs that are on the device.

NOTE: The EZM3600CB is now obsolete and replaced with newer catalog numbers, SEE the current on-line digest for new catalog numbers


CTA-ID : 2019551
Was this helpful?
What can we do to improve the information ?