Technical FAQs

Ask a Question

Are alternate mechanical lugs available for an EZM3600FS?

Yes, the standard mechanic lugs will accommodate (3) 500 Kcilm maximum per phase and neutral. For (2) 600 Kcmil Maximum per phase and neutral use an AL800MA7 and a MMLK250 for the neutral. For (2) 750 Kcmil Maximum per phase and neutral use an AL800MA7 and a MMSK2 and a TA8002N ILSO Lugs (Purchased separate). For (4) 350 Kcmil Maximum per phase and neutral use an AL1000MA and the standard neutral Lugs


CTA-ID : 2019550
Was this helpful?
What can we do to improve the information ?