Technical FAQs

Ask a Question

Is there a way to override and remove a stuck key on an XCSE7513?

The key is either misaligned or inserted too far, probably due to slamming the gate. There are warnings provided to avoid this situation in the instructions The only option is to replace the switch with new according to the instruction.

CTA-ID : 2019266
Was this helpful?
What can we do to improve the information ?