Technical FAQs

Ask a Question

What is the maximum acceptable humidity level for the enclosed 8839 Econoflex?

95% with no condensation or dripping water, comforming to IEC 60068-2-3.


CTA-ID : 2019265
Was this helpful?
What can we do to improve the information ?