Technical FAQs

Ask a Question

What is the temperature rating of a diaphragm for 9012 pressure switch

It is rated for -40 deg C to 120deg C. This is the temperature of the medium that can come in contact with the diaphram. The other components of the switch have a different temperature limitation.


CTA-ID : 2019264
Was this helpful?
What can we do to improve the information ?