Technical FAQs

Ask a Question

What are the dimension of the EZM1800CBU and the EZM1800TBU?

The EZM1800TBU is 39.98 in H 25.06 in W and 11.12 in D
The EZM1800CBU is 69.03 in H 20.46 in W and 11.50 in D

CTA-ID : 2019825
Was this helpful?
What can we do to improve the information ?