Technical FAQs

Ask a Question

What is the catalog number for a 30 Ampere, 3 Phase, 600Vac, 250Vdc, NEMA 7/9, not fusible safety switch?

Use a H60XFA for this application. The H60XFA is an enclosed molded case switch rated for 60 Ampere, 600Vac, 250Vdc maximum, NEMA 7 or NEMA 9.

CTA-ID : 2019824
Was this helpful?
What can we do to improve the information ?