Technical FAQs

Ask a Question

Are replacement contacts available for 8910DPA93?

Are replacement contacts available for 8910DPA93?

Product Line:
Definite Purpose Contactors

Products sold and used in the United States

Replacement contacts needed

In single pole kits only, order (3) 9998 DRC9 kits.

Note: Page 14-120 Digest 173 indicates that the replacement contact kit for the 8910 DPA 90A rated contactors is 9998 DRC12. This is in error, as there is no DPA 80A rated contactor. ``DPA80`` should be changed to ``DPA90``, and the last item marked ``DPA90`` should be corrected to ``DPA120``. The 120A rated 8910 DPA contactors use the 9998 DRC12 replacement contact kit, qty (1) kit per pole.

CTA-ID : 2019807
Was this helpful?
What can we do to improve the information ?