Technical FAQs

Ask a Question

What are the repair parts for the HU363AWC, series F7 (may be shown as F07)?

The repair parts for the HU363AWC, series F7 (F07) are as follows. No other parts are available.
-Line Base Assembly -4056775250 (includes all poles. Arc suppressor assembly not included)
-Line Base Mounting Screw - 4020515101(3 required)
-Arc Suppressor Assembly - 4056635550 (requires one per switch)
-Arc Suppressor Mounting Screw - 4020514501
-Lug Assembly - 4025101851 (per lug)
-Lug Mounting Screw - 4020514202 (per lug)
-Lockplate - 4056672101
-Lockplate Mounting Screw - 2299940562 (2 required)
-Handle Assembly - 4056663550 (also recommend replacing Handle Assembly External Gasket)
-Handle Assembly External Gasket - 4056603101
-Switch Mechanism - 4056787350 (also requires Switch Mechanism Washer and Interlock Gasket. NOTE: Handle Assembly External Gasket may also need replacing)
-Switch Mechanism Washer - 2360200008
-Interlock Gasket - 4056786001
-Rod/Linkage Assembly - 4056787150
-Receptacle - 2541002295
-Receptacle Mounting Screws - 4510280101 (required 4)
-Ground Lug - 4025101851 (3 total required)
-Ground Lug Mounting Screw - 4020514801 (long screw) and 4020513503 (short screw) ? 1 each


CTA-ID : 2019534
Was this helpful?
What can we do to improve the information ?