Technical FAQs

Ask a Question

What is the Equipment Ground Kit for a H361DS Series F06 safety switch?

Issue:
Selection

Product Line:
HD SS

Cause:
Accessory Selection

Resolution:
Ground lugs are provided factory installed in the H361DS (Series F01 - F07 design). The lugs will accept (2) #12 Cu or (2) #10 AL or (1) #4 max. Al/Cu conductor . To replace the ground lugs in the field, order kit GTK03 for this switch and Series.


CTA-ID : 2019522
Was this helpful?
What can we do to improve the information ?