Technical FAQs

Ask a Question

Is there a rule of thumb on number of drop hangers per foot on the LDB wireway?

Per NEC Article 362-7 space the hangers no more than 5 feet on a horizontal run, unless specially approved for supports at greater intervals, but in no case shall the distance between supports exceed 10 feet.

CTA-ID : 2019261
Was this helpful?
What can we do to improve the information ?