Technical FAQs

Ask a Question

Are the doors on the NEMA 3R MH-WP enclosures gasketed?

Issue:  
Is there a gasket on the NEMA 3R panelboard enclosures such as the MH-WP boxes?  

Product line:  
NEMA 3R panelboard enclosures

Environment:  
MH-WP style panelboard enclosures

Resolution:  
Yes, they have a gasket on the door which is required for them to be classified NEMA 3R.  
Was this helpful?
What can we do to improve the information ?