Technical FAQs

Ask a Question

What is the interrupting rating of the ML-1 breaker p/n 989720?

The ML-1 breaker was rated 14K at 480V and 240V.


CTA-ID : 2020236
Was this helpful?
What can we do to improve the information ?