Technical FAQs

Ask a Question

What was software revision S264 on the ATV66D23M2S264 drive and is it a direct replacement for the standard drives?

According to PLE this is a direct replacement for the ATV66D23M2, it provides a greater range of setting up the full load current than the M2 drive. This unit along with all ATV66 are currently obsolete.


CTA-ID : 2020233
Was this helpful?
What can we do to improve the information ?